Demo Mode

You can use the Advanced Power Application Suite without a software license in Demo Mode, which enables you to preview the application's features without connecting to an actual instrument.

Some functionality shown in the Demo Mode may not be available on your particular instruments.

1. To enable or disable Demo Mode, click the Select Instrument drop-down.

2. Toggle the Demo Mode switch.